InnoTrans 2016: HARTING presents innovative rail solutions
HARTING Technology Group has a long tradition with the railway sector which continues to grow in importance due to the company’s global orientation. Rolling stock offers outstanding potential as a means of transport both in urban centres as well as over long distances, as in US or South Africa, for example. Consequently, HARTING is optimistically viewing the InnoTrans trade fair slated to run this September 20-23 in Berlin.
HARTING will be using its stands at the event (Hall 12, Stand 203 and Hall 4.1, Stand 426, Berlin Exhibition Grounds) to present its innovative products, systems and application solutions for the railway sector, with the HARTING MICA to be showcased as well. The HARTING MICA, a modular computer unit specially designed for use in industry, was honored with the HERMES AWARD at the Hannover Messe trade fair in April 2016.
At InnoTrans, HARTING will be demonstrating how digitalization, modularization, miniaturization and integration can be optimally implemented in the railway environment. For example, the MICA aggregates the communication content of the RFID system and enables direct and decentralized analysis and data preparation, as well as data format conversions. “These data are then furnished to a central unit.
In addition, HARTING will use InnoTrans to present to the specialist audience the capabilities of the new Han® 34 HPR EasyCon railway connector. This connector performs well even in limited space in the gangway area, and also to present a new interface for IGBT controls in a space-saving DIN housing.