Miniaturized solution for rapid placement of connections
Automated processing of components is steadily increasing. HARTING is keeping up with this trend with the M12 SMT, which can be seated on the circuit board using pick & place – automated and fast.
The automated assembly of printed circuit boards is expanding to include ever more components. While formerly limited to just a few parts, today virtually all the components of a circuit board can be loaded using pick & play. These are then all heated in a soldering furnace and soldered. This eliminates the need for separate wave soldering and consequently saves costs.
HARTING is keeping up with this trend with the M12 SMT, which will be available in codes A, D and X in male and female versions. This move will bring both power and Ethernet up to 10 Gbit/s to the PCB from new miniaturized switches.
The distinct advantages of this are the automated, rapid and more cost-effective placement of the connection, since dispensing with through-hole contacts means it can now also be equipped on both sides. The result is a miniaturized solution that is faster and less expensive to produce.
The connection is slated to be rolled out in the autumn of 2016.