INDUSTRY SEGMENT - Automotive
Electromobility for the future
HARTING Automotive develops and produces charging equipment for electric and plug-in-hybrid vehicles. Our products have the approvals and certificates relevant for all specific market sectors and legal requirements worldwide.
HARTING provides robust, reliable, and user-friendly solutions for the entire Well to Wheel supply chain.
From our triad of Installation Technology, Device Connectivity and Smart Network Infrastructure, HARTING provides suitable products for power, signal and data transmission. Our industrial connectors, Ethernet switches and charging plugs and sockets are numerously deployed in applications of energy production, in distribution networks and the charging interface for electric vehicles.
HARTING | Much more than just connectors.
"Using state-of-the-art technology combined with our customised and environmentally friendly strategies and solutions, we will work together with the auto industry to meet the challenges of tomorrow's mobile traffic," explains Marco Grinblats, Managing Director of HARTING Automotive.
Automotive industry
In automobiles, HARTING Automotive is represented in a wide variety of applications with its solenoid systems: steering systems, circuits or locking and safety technology are just a few of the many elements that must function safely and reliably in vehicles. So it is with good reason that companies from the automotive and supplier industries rely on quality products from HARTING Automotive.
![slider automotive slider automotive](/sites/default/files/2021-11/Silder%20Automotive.jpg)
AC Mode-3 charging cable HARTING offers straight and coiled Mode-3 charging cables for mobile charging at public charging stations. These cables are available in different lengths.
- Ergonomic and functional design that fits well in the hand.
- Approval for all common standards and requirements worldwide.
- Large product portfolio with different cable lengths and cable types.
- High product quality due to many years of experience in the field of charging cable production.
- Local and European production sites meet price and volume expectations.
- VW Group Award 2020 winner for first-class service in the OEM business.
- Design and layout (logo, colour, length, etc.) can be adapted.
In addition to individually configurable Mode-4 charging cables with open ends, HARTING also offers charging sockets and plug holders. Like the charging cables themselves, the cable connections of the charging socket can also be individually designed.
- Ergonomic and functional design that fits well in the hand.
- Approval for all common standards and requirements worldwide.
- Large product portfolio with different cable lengths and cable types.
- Two hands are not required to open the charging socket hinged cover (one-hand operation).
- High product quality due to many years of experience in the field of charging cable production.
- Local and European production sites meet price and volume expectations.
- VW Group Award 2020 winner for first-class service in the OEM business.
- Design and layout (logo, colour, length, etc.) can be adapted.
Charging socket, type-2
AC charging socket for charging electric vehicles
- Installing in an AC charging station or wall box.
- For charging electric vehicles with AC power for the European market.
- Only to be used together with the charging cables provide with type-2 charging plugs, in accordance with IEC 61851-1 and IEC 62196-2.
Wallboxes & charging stations
In addition to charging cables and charging sockets, HARTING offers a wide portfolio of additional components that can be used in the charging station or wallbox sector.
3D-MID solutions in automobiles
Assistance systems, safety features or infotainment – more and more electronics are finding their way on board today’s cars. You can fit complex electronics into your car even where space is at a premium.
Light sensor for controlling air conditioning systems
Modern air conditioning systems control the interior temperature depending on various influences for example the exposure to sunlight.
To increase measurement accuracy, HARTING has developed a space saving base carrier that enables precise 3D arrangements of the optical sensors.
Lighting module for vehicle interior
Modern lighting systems integrate classic interior lighting and reading light in one module.
With the MID component from HARTING, it was possible to develop a lighting module with a compatible interface that enables a cost reduction of 35 % compared to the previous solution with a significantly lower installation height and reduced number of parts.